Hello,
Setting the High speed mode is clear in the data sheet, but how can I set this device to Standard Mode Vs Fast mode?
thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
There is no standard vs fast but joint standard-fast only. The master is clocking the bus with up to 400 [kHz] in standard-fast mode but it means that 100kHz will work as well. I might be wrong but i suspect other clocks under 400 [kHz] to work too.
Regards,
Maciej
Hello F, good to hear from you.
The Standard and Fast Modes are controlled by the i2C controller (master). The ADC081Cxx determines the FAST or STANDARD speed based on the timing specifications on page 8 of the datasheet, then will respond in like mode.
-Leonard
p.s. . . there is Stellaris source code that implements this fast-standard vs. HS protocol: http://e2e.ti.com/support/microcontrollers/stellaris_arm/f/471/p/235977/827110.aspx#827110
-Leonard