Hi all,
It is DAC34SH84 and requested the current waveform.
What does it become on condition of the following?
fDAC = 1.5 GSPS, 4× interpolation,
mixer on, QMC on, invsinc on,
PLL disabled, 20-mA FS output, IF = 500 MHz,
Within DACA/B/C/D、used to DACA/B.
Used High Speed Data Converters Forum: RE: About the power consumption of DAC34SH84 forum.
best regeards,
Hisa Kobayashi.