Hi
I'm using a REF3220 to provide the reference voltage to a DAC7718 with OUT_F and OUT_S tied together since the trace length is only about 2cm. The ENABLE pin is pulled down to GND and is raised to +5V by a microcontroller to adhere to the DAC7718 power cycle requirements. Usually everything works just fine. However, sometimes (about 1 out of 5) times when I apply power to my board, after the microcontroller enables the REF3220, the voltage at the REF3220 output will be between 2.080V and 2.100V albeit stable. The REF3220 will continue to output this voltage even if I power cycle repeatedly and appears to be stuck here. I'm making measurements with an Agilent 34410A.
Do you have any suggestions of possible causes for this behavior?
Schematic:
IN - bypassed with 1uF ceramic cap then through a ferrite bead then to the +5V output of a LDO regulator
ENABLE - tied to GND via a 47k resistor and connected to output pin of microcontroller with +5V logic levels
OUT_F + OUT_S - tied together and connected in series with a ferrite bead and then the DAC7718 VREF pins
GND_F+GND_S - tied together and connected to GND
Thank you!