Hi all
There is a question by setup of DAC5689.
Table 5. Register name: CONFIG3 Address: 0x03, Default 0x00
Bit 7 Bit 6 Bit 5 Bit 4 Bit 3 Bit 2 Bit 1 Bit 0
diffclk_dly(1:0) clko_dly(1:0) Reserved
0 0 0 0 0 0 0 0
Although I am as mentioned above,
How is CLK2 set up if above-mentioned diffclk_dly is set as 1ns, 2ns, and 3ns?
Moreover, Figure28 of CLOCK MODE What does delta<t_align become?
For example, it is t_align=190ps when it is CLK1=112 MHz and CLK2= 672 MHz.
Unless it sets delta to less than 190 ps, can't it go then?
Moreover,
diffclk_dly (1:0) is the function (0 or 1 ns, 2 ns, 3 ns) to set up the delay time of the input of CLK2/CLK2C (672 MHz).
clko_dly (1:0) is the function to set up the delay time of CLK1 (112 MHz).
Is it what may be considered?
Best Regards,
Hisakichi Kobayashi.