Hi ppl,
Can some1 suggest an ADC with the following features :
1 . It should have two channels
2. Minimum Sampling rate of 10MHz
3. Resolution 24 bits. Input signal will vary from -2V to 2 V.
4. Both the channels should be acquired simultaneously. I am trying to measure the phase shift between a pair of signals. Hence, simultaneous acquisition is of at-most importance.
5. Power Consumption is not a big issue, as this project is in the research phase only.
Regards,