Hi,
I using ads7843 touch converter IC. Is there any drive ads7843.c use SPI code by GPIO available for this IC ?
I find this code example and use is for msp430g2533 but the return data x and y not correct.
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Khoa,
Here is something I have just found.tsc2046_reference_firmware.zip
Actually it is reference firmware code for TSC2046. Since TSC2046 is 100% pin-compatible with the ADS7846 and ADS7846 is 100% pin-compatible with the ADS7843. This code should be OK for ADS7843.
ADS7846
Andy