Hi,
What High Speed Data Capture and Pattern Generation Platform should be used with the DAC5688 and DAC5589?
The Customer has a TSW1400EVM, but it doesn’t look like the TSW1400EVM supports the DAC5688 and DAC5589.
Thanks,
James
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi James,
TSW1400EVM will work with the DAC5688/89 EVMs. You have to select cmos from the device list as shown in the picture below to load the firmware.
Here is the updated section 6: DAC5668/88/89EVM initial Power Up and test.
DAC5668/88/89EVM Initial Power Up and Test
The steps described in this section show how to connect and configure the DAC5668/88/89EVM for evaluation under the default settings.
You should be able to use the user guide for the DAC5688 EVM for rest of the configurations. Below is the link for the user guide.
http://www.ti.com/lit/ug/slau241a/slau241a.pdf
Regards,
Neeraj