Other Parts Discussed in Thread: THS1206
We are using THS1206 for data acquisition.
Data acqusition is happening well when input is given from function generator i.e. 1.5V to 3.5V.
But, when input is given from the actual source of interest, ADC is not functioning in full range.
i.e not giving the digitalized data corresponding to 2v i.e. from 1.5V to 3.5V ( 0 to 4096 ).
Getting digitalized data corresonding to 1V ( even though 2v signal ranging from 1.5v to 3.5v is given as input ).
That too, base line also is shifting from 2.5V to approaximately 1.8v.
What can be the reason?
I would like to have effective data conversion for 2V.
Base line shall be at 2.5v.
Pl suggest what precautions and changes have to be made to get full scale & to get base line at 2.5v.