Hi,
I am using DAC8234 to generate bias voltages for power amplifiers. The required output voltages are (-5V to -2V) and +17.7V.
I have selected AVdd as +22V and AVss as -12V. REF-A and REF-B pins are at 5V. IOVdd is 3.3V and DVdd is 5V.
Could some one please tell me the maximum current consumption on the below mentioned pins?
AVdd, AVss, DVdd, IOVdd, REF-A and REF-B
Thanks in advance
Nithesh