HI,
We have an FPGA as I2C Master interface to the ADS1115 device. We would like to configure the device with 2 single-ended or 2 differential inputs.
Is it possible to switch the Input multiplexer live between two conversions if the device is configured in "continuous conversion" mode?
using with the following sequence:
1) Configure AIN_0, read dummy data when ALERT/RDY asserted
2) Configure AIN_2, read data from AIN_0 when ALERT/RDY asserted
3) Configure AIN_0, read data from AIN_2 when ALERT/RDY asserted
4) goto 2)
From our test, it looks like the device keeps providing converted data from only one of the 2 inputs, AIN_0 or AIN_2.
Note: I found a thread with somebody asking a similar question for the ADS1118 but I couldn't see the confirmation for the "continuous conversion" mode.
Thanks,
Denis