This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I've been thinking different options for a case where there might be one or optionally two ADS131A04 and those needs to be synchronized. This is a case where there always is one analog input daughter card present, but then optionally there might be also second daughter card installed. I first thought that from system perspective perhaps easiest to manage would be to use both in synchronous slave mode. However I did not find from datasheet that how accurate the synchronization pulse on DRDY input must be related to CLK_IN to avoid resynchronization / filter reset.
I found a thread where it can be interpreted that this pulse actually needs to be exactly on correct CLK_IN edge. Is this correct or is there any range when the pulse may be given without resetting the filters. Also what is the maximum length of this pulse, is it one CLK_IN cycle? Datasheet says also that "In synchronous slave mode, DRDY is an input signal that must be pulsed at the device set data rate". So if would give just one falling edge to to DRDY for devices to be sychronized and then keep signal low, would that also cause resynchronization fault? (of course in this case it could happen that some data is missed when reading is not keepin in synch, but that would not be that serious as resynchronization fault).
I was just wondering that if it must be very exact and ADCs are running on different clock than controlling host, then reaching a system with where all ADCs are in synchronous slave mode and there would not happen resynchronization faults will be hard.