Hi all,
My customer plans to use ADS52J90 for a photo sensor input application.
A signal path is as follows;
Photo sensors -> I/V conversion of a photo diode input (OPA2300) -> single to differential conversion (THS4509) -> ADS52J90
Input channels are 32, so that the sampling rate is 50MHz.
All signal path is DC coupling.
The photo sensors signal band width is from DC to >10MHz (or 20MHz; not fixed yet).
Questions are;
1. For considering LPF, what is the differential input resistance and the differential input capacitance of ADS52J90?
2. Could you give me your advice about the LPF design?
- According to Anti-Aliasing Calculation Tool for A to D Converters , the required attenuation is -61.96dB and the number of Filter Poles is 14.
I feel it's hard to design for realizing the LPF by analog method. Is my understanding right?
If no, could you tell me the recommended analog LPF for 50MSPS?
If yes, should be done by digital LPF after conversion? In this case, what is the recommended LPF for ADC?
Regards,
Toshi