This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I want to ask about Fig 111 ..page 81
I want to use ADS131 with AVss on GND AVdd=5V Vrefex= +5,000V IOVdd= 3.3V
I found for this case the example figure 111 wrong : It should be AVSS and VNCP on Ground and AVDD should be wired on +5V
correct?
best regards
zbyno
Hi Brain,
1. Thank you fo your answer...
2. Can ADS131A04 work with Fmod 4,8MHz? With Fin = 19.2 MHz
I need to have Fdata .....100 kSmpl by OSR 48.. see table3 on page 22
thanks
zbyno