This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, when negative charge pump enabled, we can accept as low as AVSS-1.5V input at VINP and VINN.
So when I apply AVDD=3V, VREF=3V, VINN=1.5V, VINP ranges from -1.5V to 1.5V, the ADC can still work well, right?
The only bad effect is that the input is equal to -3 to 0V range, so the corresponding digital output will not be full scale, only 0-2^23, right?
Hello Howard,
Thank you for your post.
The negative charge pump allows the absolute input voltage to range from AVDD to (AVSS - 1.5 V). For VINN = 1.5 V, the differential input voltage will never be positive if VINP = -1.5 V to 1.5 V.
If you are looking to utilize more of the ADC full-scale range, you should connect VINN to GND. The differential input voltage would then be equal to VINP (+/- 1.5 V).
One detail that needs attention in the configuration you described is the reference voltage. VREF = VREFP - VREFN must remain 500 mV less than AVDD. For AVDD = 3 V, the maximum reference voltage you can use is 2.5 V.
Best Regards,
Ryan,
thank you.
But according to datasheet, Vcm should be within AVSS and AVDD, so when Vinp ranges from -1.5 to +1.5, I can only set Vinn=1.5 and keep the differential input voltage to be -3 to 0.
In this state, I can still use this device with some constraints(no positive differential input).
If I keep Vinn=0, I can't use this device, right?
Hello Howard,
The input common-mode range should match the analog input range. When the negative charge pump is enabled, the input common-mode voltage can range from AVSS - 1.5 V to AVDD.
Best Regards,
Thank you.
So I'll tell the customer that they can use the device as you mentioned.