This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi,
I am using the ads131a04 to sample 4 channel analog signals. I have at least two problems reffering to the vref and digit outputs. I am using the internal refference voltage and Bipolar Analog Power Supply. the Negative Charge Pump is disabled. please see the attached schematic, where VCC is 2.7V and VEE is -2.7V.
1. REFP is not as expected. when I set it to 2.442V(or after powering up), What I get is about -1.3V; when I set it to 4.0V, What I get is about1.6V;
2. The digit output is hard to explain. When a DC voltage of about -0.5V is applied to the AIN?P, the output code is 0xED?? or 0xF0??. It seems like there is a big DC offset in the output code. I have failed to find how the output codes is related to the input voltage and the refference voltage, in the datasheet.
thank you!