Part Number: ADS131A04
Other Parts Discussed in Thread: ADS131A02
Hello,
I use this device with an analog supply of AVDD = + 2.5V and AVSS = -2.5V. Chapter "10.1.1 Unused Inputs and Outputs" states that unused analog inputs shall either be left floating or tied to AVSS.
My question is: which one is the preferred method? Is there any advantage of using one over the other?
Only in case connection to AVSS is the preferred method:
In that case, due to a more convenient layout, i would like to connenct unused analog inputs to GND (which in my case is about half way between AVDD and AVSS). My understanding is that this should be equivalent to the connection to AVSS. Is this assumption correct? Or may there be unforeseen problems (e.g. during power up/down if AVSS temporarily goes slghtly above GND)?
As for the ADS131A02: Does it have the same die as the ADS131A04? Are the NC pins 5 to 8 internally bonded to the die?
Thanks and best regards!