Hello,
I would like to use DAC12C085 with 2.5V full scale.
Thus, we use 3.3V for Va and 2.5V for Vref.
However in the datasheet P.26 there is the description that "To use the full dynamic range of the DAC121C085, the supply pin (VA) and VREF can be connected together and share the same supply voltage.".
I couldn't understood this description.
Can we use this device with 2.5V full scale range with 2.5V Vref voltage?
Best Regards,
Ryuji