This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello team,
Hope you are well. Would you be able to help out with customer question below:
When the CS input is LOW I am assuming that the DOUT/DRDY signal drives both HIGH and LOW. (complementary output drive in both directions)
This would seem to be the standard way to doing things but when I read the PULL_UP_EN section of the “Table 7 - Config Register Field Descriptions” I became a bit confused over the sentence: “This bit enables a weak internal pullup resistor on the DOUT/DRDY pion only when the CS is high.”
I am assuming that when CS is LOW the weak pullup is overdriven by the DOUT/DRDY output pin driver. Is this true?
I am also assuming that the weak pullup is made available so that it keeps the DOUT/DRDY signal PCB trace from floating when the ADS1118 is an idle not transmitting data.
Randhir,
The weak pull-up resistor is enabled only when /CS is high. Without the weak pull-up, the DOUT/DRDY is normally in a high-Z mode and could potentially float high or low.
When the /CS pin is low, the DOUT/DRDY actively drives the output high or low, without the use of the pull-up.
Joseph Wu