This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC3484EVM: DAC3484EVM: Need clarification on DAC348XEVM-SCH_H Schematics

Part Number: DAC3484EVM

Hello All,

I am designing a custom board based on high speed DAC DAC3484 , using DAC348XEVM-SCH_H Schematics as a reference.

Referring the schematics , Part U2 - CDCE62005 - pin 16(U2P) : DACCLKC  is connected to U1-DAC3484- pin B3 (DACCLKN)

& Similarly Part U2 - CDCE62005 - pin 17(U2N) : DACCLK, is connected to U1-DAC3484- pin A3 (DACCLKP)

This looks like P&N of the CDCE62005 is connected to N&P of DAC3484, is this right way? (Because other  P&N signals coming out of DAC3484 orCDCE62005 are connected in a matched way ). Datasheet of CDCE62005 says its outputs are user definable

Please suggest at the earliest.

Thanks&Regards,

Shyamsundar