Other Parts Discussed in Thread: TIDA-00498, TIDA-00834, TIDA-00128, TIDA-00493
in the article , tiduco9a.pdf,I have some question below
first,in the table 3,I want to know how to decide the value the load resistor which is 13.778,why it not 30 or other?for example,I know the max input 7.07 from 10/1.414) why make the op gain is 9.92 why the primary current is 129.318 A ,why not 120A,why how dose these data get from?
second, about the two stage RC filter,which frequency do they filter ,is there a article describe more detail?
third ,for example if my ADC input max voltage is 0~3.0V,what the range of the op output is fit?0.5~2.5 or 0~3 or 0~2.5,now my cicuit below ,the output of the op is 0.5~2.5,I have no idea。IF i want to get a range from 0~2.5V,how should i modify the circuit above?how to select the burden resistor?my primary current is 50hz AC 1A~5A .the RC filter between the two op,how to decide the value?different circuit has different resistor to obtain gain,is there any principle to obey to decide the value of the resistor?
fourth,I found that in the circuit above the signal out from transformer go into the positive pole of the op。
but in the the circuit below ,the signal out out from transformer go into the negative pole of the op,why?which has a better performance?