Hello support team,
I have some questions regarding DAC8411.
Our customer is carring out the noise testing with DAC8411, and a strange phenomenon has occurred.
Operating the DAC8411 with noise superposed on the AVDD / VREF line results in an output waveform in which only MSB data is inverted due to malfunction.
Although the input digital data is straight binary, it seems that two's complementary circuits are operating as far as we see the analog output waveform.
We heard that it is easy to reappear by experiment as follows.
a. Apply a sine wave of 100 kHz, center voltage of 3 V, and amplitude of 2 V to AVDD / Vref.
b. Gradually lower the center voltage and set it to about 1.5 V.
c. Set the amplitude to 0 V and the center voltage to 3.3 V.
[Questions]
1. Is there a two's complement mode in DAC8411 (as a hidden mode)?
2. If there is a two's complement mode, what is the trigger to enter this mode?
3. If this mode is entered, is there any way to escape from this mode besides turning off and on the power supply?
Sincerely,
M. Tachibana