This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I need a 2.4GHz clock to drive a DAC5670. Can somebody point me to an application note which describes the best method to generate this clock?
Do I also need to use a jitter control IC?
Richard, the DAC5670 is supported out of the HiReliability group.
We do not have an app note on clocking the DAC5670 at this time. I do know that the CDC versions of clock drivers are not capable of operating the DAC5670 at max speed of 2.4Ghz. I will work with our RF team to see if we have an integrated solution that we can provide.
Regards,
Wade