Im working with ADS 1298 and NRF52832 from Nordic, i have a problem when i tried to read the ID control register( 00H ), i just get random values, maybe the problem is the SPI between the ADS and NRF52, i test the SPI of the NRF with arduino and it works well, i used 128Khz for the test, whit the ads i used 128K,250K,500K,1M,2M,4M,8M and its the same, i tried to read the ID control register before configure any other register. Can you help me?
what is the frequency of the SCLK? would i have to wait every byte that i send or recieve?