Hi,
Could you please confirm that the DAC8563T DAC default output voltage after power on is 0V? It is specified that at reset, the reference is set to external by default (which would be 0V if no external reference is used) and the gain is 1 by default. Since the part reset DIN to mid scale, I assume I would have an initial output voltage of Vref/2 = 0V / 2 = 0V. Am I right?
Is it possible to set up the DAC so that it defaults to 2.5V at power on? I would like to have a +/-5V output using an opamp as described in the following TI verified design circuit http://www.ti.com/lit/ug/slau525/slau525.pdf but I need to ensure the output is 0V at power on.
Thanks