Part Number: ADS4222
Other Parts Discussed in Thread: THS4509,
Hi,
I want to use ADS4222 for digitizing sensor signal which ranges from 0.9V to 1.8V.
The sensor can drive load of 1K and above. The bandwidth of the input signal is from DC upto 20 MHz.
Please suggest an input drive circuit for the above application.