This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Greetings,
I am using DAC38J84 EVM REV D to evaluate the DAC. I find that the output goes fully noisy probably due to SERDES PLL being out of lock whenever 8 SERDES lanes are are used. I need to operate the DAC at an input rate of 1000 MSPS for generation of DVB-S2X signals and am using an external clock and an interpolation rate of 1X. The EVM works fine at DAC input rates below 620 MSPS and while 4 SERDES lanes are used. I just used the 'Quick Start Menu ' on the GUI to configure the settings. The settings on the quick start menu of 'DAC3XJ8X GUI V1.1' are as below:
EVM Clocking Mode: External Clock
Device: DAC38J84
Number of SerDes Lanes: 8
DAC Data Input Rate: 1000 MSPS
Interpolation: 1
DAC Output Rate: 1000 MSPS
FPGA Clock: 250 MHz
JESD204B Mode (LMFS) : 8411
SerDes Linerate: 10000 Mbps
Thanks and Warm Regards,
Prasidh