I am using ADS8695 in my project.
2. The IC is functioning properly at room temperature. But when i am soaking it at 71 degC, the outputs are getting stuck to their higher values (approx. double of the input). In this case inputs are not deviating from their values.
3. The IC has been configured in the range of 0-5V and the inputs are being given in the same 5V range. The IC is interfaced with ST Microprocessor on SPI interface.
4. Is any pull-up/pull-down is required for SPI clock that is coming from ST Microprocessor?
5. I am utilizing only 12 bits of this ADC, is this creating the issue?