Hi,
My customer have a question.
In table 6 of the datasheet of ADS8900, No. of SCLK is 20, but Figure 60 shows 22 CLKs. Which is correct, 20 CLKs or 22 CLKs? If 20 CLKs is corrrect, does SDO packet starts from D19 in Figure 60 ?
Similarly, In table 7, No. of SCLK is 5 in quad mode, but we can see 6CLKs in the packet for quad mode in Figure 66. Which is correct, 5 CLKs or 6 CLKs? If 5 CLKs correct, Don't the D21 and D20 exist in the packet of Figure 66 and Is the MSB D19?
Best Regards, Taki