Other Parts Discussed in Thread: ADC34J44
Hello,
I have two issues with the board.
1. Working with lower sampling rates
I am working with the ADC34J44EVM and TSW14J56EVM for data acquisition.
I am using the ADC3000 GUI and HSDC Pro software.
I have used the following configuration file provided along with the ADC 3000 GUI to initialize the ADC board.
'ADC3xJxx_80MSPS_Operation_LMK_Setting.cfg'
This operates the board at 80MSPS and I could acquire the data from the TSW14J56EVM.
I need a way to work with lower sampling rates, e.g. 5MSPS or 10MSPS.
How do I configure the board for my application?
2. Problem in acquiring lower frequency signals
I have tested the board for various frequencies ranging from 1kHz to 10MHz at channel B using a function generator.
I acquired the data using the 80MSPS configuration file mentioned above.
I found that for frequencies lesser than 300kHz the signal started to attenuate.
How do I work with smaller signal frequencies (1-50kHz) without attenuation?
Regards,
Sudeep