Hello,
My customer have some questions about TX517.
[Q1]
"Disallowed logic states" is listed in Table 2 in the D/S.
I agree that the "disallowed mode 1" and the "disallowed mode 2" are not allowed because these are a short-thru fault condition.
"Example input data set of a 17-level output" is listed in Table 3 in the D/S.
There are some disallowed logic states in this table.
For example, I think that "output level 6" corresponds to "Disallowed mode 2" because INP0B and INN0B are ON.
How do I interpret this?
Can I think that INP0x and INN0x will allow "short-thru" fault condition ?
[Q2]
TX517 can generate 5-level output for single-ended.
Is my understanding correct ?
<My understanding>
output level 2 : INP1x=ON, INN1x=OFF, INP2x=OFF, INN2x=OFF, INP0x=OFF, INN0x=OFF
output level 1 : INP1x=OFF, INN1x=OFF, INP2x=ON, INN2x=OFF, INP0x=OFF, INN0x=OFF
output level 0 : INP1x=OFF, INN1x=OFF, INP2x=OFF, INN2x=OFF, INP0x=ON, INN0x=ON
output level -1 : INP1x=OFF, INN1x=OFF, INP2x=OFF, INN2x=ON, INP0x=OFF, INN0x=OFF
output level -2 : INP1x=OFF, INN1x=ON, INP2x=OFF, INN2x=OFF, INP0x=OFF, INN0x=OFF
[Q3]
They seems to want fast rise/fall time.
Therefore they are considering whether it can be used as follows.
<case 1>
HV1=40V, HV2=40V, HV0=5V
LV1=0V, LV2=0V, LV0=0V
Is this configuration possible ?
<case 2>
HV1=40V, HV2=40V, HV0=5V
LV1=-30V, LV2=-20V, LV0=-5V
Is this configuration possible ?
[Q4]
They are considering whether to be Single-ended or Differential.
Is my understanding correct ?
<My understanding>
Differential has the following advantages compared to Single-ended.
1. Higher output voltage
2. up to 17 levels output (Single-ended is up to 5 levels output)
3. Better common-mode noise
Differential has the following disadvantages compared to Single-ended.
1. Require many power supply voltage
2. Only 1 output
Are there other advantage / disadvantage ?
Best Regards,
Hiroshi Katsunaga