This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC38RF89: SPI bus

Part Number: DAC38RF89

Team,

My customer has the following question on the SPI Bus Rate for the DAC38RF89.  The datasheet says 10 MHz (section 7.9).  On another program with an "older" DAC they had the same issue and were told, I'm guessing since it is a nominal value not a MAX, that running it faster (say 20 MHz) shouldn't be a problem.  Is there a way to confirm the same for this DAC?

Regards,

Aaron