What is the output data format and LSB size of the ADS1258 or ADS1158 devices?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
For assistance in scaling the ADS1x58 output data, here is the data formatting table and equation for the LSB size:
NOTE:
The output codes from the ADS1x58 are 2's compliment (signed) values. 24-bit signed for the ADS1258, and 16-bit signed for the ADS1158.
Therefore, 0xFFFFFF (hex) = -1 (decimal) for the ADS1258, and 0xFFFF (hex) = -1 (decimal) for the ADS1158.