This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE4405EVM: The eval board stopped working. Software issue

Part Number: AFE4405EVM
Other Parts Discussed in Thread: AFE4405

I cannot get my AFE4405EVM GUI to work any more. It worked before but now the GUI exe cannot get connected to the board. I get an error message "An error occurred while communication with the device". The state of the program is "Update Interface at Init" when the error pops up.

I have tried to re install the software but it does not help. The issue started after I installed another software (TDC1000-TDC7200EVM software), that still works.

I have also tested to run the AFE4405 eval board on my colleagues computer and that works fine. Thus, no issue with the hardware 

Anyway, the USB driver looks good when the board is connected and I can update the FW using the exe (BSL_USB_GUI.exe).

I have LabVIEW (64-bit 2017) installed on my computer. VISA version 17

I use Win7, 64 bit.

What to do?