This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ti Experts,
We have a project which used to leverage ADS1299-8 for data acquisition. Due to change in technical requirement , we decided to migrate it to ADS1299-4 instead. Apart from the difference in number of available adc channels between the two parts, is there any other differences? We tried to plug in ADS1299-4 on our development board which used to house ADS1299-8, we noticed that the firmware driver we developed for ADS1299-8 doesn't work on ADS1299-4. As far as we know, both chipset are protocol compatible, thus firmware should be compatible as well.
Best regards,
Peter