Hello,
Currently I’m reading the ADS1220 with ppi in single-shot mode with 600 Hz, which works fine.
With a tx-buffer I’m sending the Start/Sync, READ DATA command and reading the data (tx_buffer = [0x08, 0x10, 0xFF, 0xFF, 0xFF])
The Problem:
I connected the bridge GND to AIN03 and set the Low-side power switch to automatic, to reduce power consumption.
I expand my tx-buffer with the Power-Down command to open the Low-side power switch after conversation.
Now I’m getting corrupted data …
Is it possible to open the Low-side power switch between conversations?
Greetings
Arthur