This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am recently trying to simulation the data chain from ADC digital Output to FPGA, I am using the ADS5401 IBIS model and encounter issues when importing the model into HyperLynx.
Could you help me to take a look at the issue and see if there are any suggestions? I am using HyperLynx V9.4, and the model editor report errors as following:
Users/ibs79A3.tmp/ads540x.ibs(6330) : Error : Pin model SeriesR used by the series pin mapping from pin P10 to pin N10 of component ADS5401ZAY does not exist in this file.
Users/ibs79A3.tmp/ads540x.ibs(6330) : Error : Pin model SeriesR used by the series pin mapping from pin P5 to pin N5 of component ADS5401ZAY does not exist in this file.
Users/ibs79A3.tmp/ads540x.ibs(6330) : Error : Pin model SeriesR used by the series pin mapping from pin P3 to pin N3 of component ADS5401ZAY does not exist in this file.
Users/ibs79A3.tmp/ads540x.ibs(6330) : Error : Pin model SeriesR used by the series pin mapping from pin P2 to pin N2 of component ADS5401ZAY does not exist in this file.
Users/ibs79A3.tmp/ads540x.ibs(6330) : Error : Pin model SeriesR used by the series pin mapping from pin P1 to pin N1 of component ADS5401ZAY does not exist in this file.
Users/ibs79A3.tmp/ads540x.ibs(6330) : Error : Pin model SeriesR used by the series pin mapping from pin M4 to pin M3 of component ADS5401ZAY does not exist in this file.
Users/ibs79A3.tmp/ads540x.ibs(6330) : Error : Pin model SeriesR used by the series pin mapping from pin M2 to pin M1 of component ADS5401ZAY does not exist in this file.
Users/ibs79A3.tmp/ads540x.ibs(6330) : Error : Pin model SeriesR used by the series pin mapping from pin M5 to pin L5 of component ADS5401ZAY does not exist in this file.
Users/ibs79A3.tmp/ads540x.ibs(6330) : Error : Pin model SeriesR used by the series pin mapping from pin L4 to pin L3 of component ADS5401ZAY does not exist in this file.
Users/ibs79A3.tmp/ads540x.ibs(6330) : Error : Pin model SeriesR used by the series pin mapping from pin L2 to pin L1 of component ADS5401ZAY does not exist in this file.
Users/ibs79A3.tmp/ads540x.ibs(6330) : Error : Pin model SeriesR used by the series pin mapping from pin K4 to pin K3 of component ADS5401ZAY does not exist in this file.
Users/ibs79A3.tmp/ads540x.ibs(6330) : Error : Pin model SeriesR used by the series pin mapping from pin K2 to pin K1 of component ADS5401ZAY does not exist in this file.
Users/ibs79A3.tmp/ads540x.ibs(6330) : Error : Pin model SeriesR used by the series pin mapping from pin J4 to pin J3 of component ADS5401ZAY does not exist in this file.
Users/ibs79A3.tmp/ads540x.ibs(6330) : Error : Pin model SeriesR used by the series pin mapping from pin J2 to pin J1 of component ADS5401ZAY does not exist in this file.
Users/ibs79A3.tmp/ads540x.ibs(6330) : Error : Pin model SeriesR used by the series pin mapping from pin H4 to pin H3 of component ADS5401ZAY does not exist in this file.
Users/ibs79A3.tmp/ads540x.ibs(6330) : Error : Pin model SeriesR used by the series pin mapping from pin H2 to pin H1 of component ADS5401ZAY does not exist in this file.
Error : Parse failed on file Users/ibs79A3.tmp/ads540x.ibs.
C:\Users\NEOSIL~1\AppData\Local\Temp\ibs79A3.tmp\ads540x.ibs - 127 error(s), 127 warnings(s)
Thanks ahead!
Hi Yusuf,
Please contact the product group about this model. They used Teraspeed to create a measurement based model.
We did not participate in the creation of this model.
David
I have an additional question regarding to this model:
The description of Differential LVDS Output in the IBIS model is shown as following:
But to my knowledge that most of the series LVDS series termination resistor is 25 to 75ohm, this model is using 2k as default value, I am curious is there a reason for choosing this particular value?