This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC1305L25: Single End Communication

Part Number: AMC1305L25
Other Parts Discussed in Thread: SN65LVDT14, AMC1305M25, SN65MLVD203B

1. Is AMC1305L25 able to be configured as single-end communication when both CLKIN_N and DOUT_N pin are connected to ground? Or only LVDS communication is used?

2. Is SN65LVDT14 only one transceiver for the AMC1305L25 communication with C2K/MCU?

Regards

Brian W