This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM98555: Driver Ground pin of LM98555 connected to Vref to generate driver of +5V to +1V / +2V

Part Number: LM98555

Dear All,

For One of the application I want to use this IC to generate signal between +3.3V and Ground to converted to +1V to 5V  or +2V to 5V.

So question is Will this IC generate this wave form of +5V to +1V by connecting it to +1V/+2V at GNDO pin of driver? 

Thanks in advance 

Abhishek