This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS5294EVM: Current drawn by ADS5294 EVM

Part Number: ADS5294EVM
Other Parts Discussed in Thread: ADS5294

hi all,

we are facing an issue with the ADS5294 EVM .

The current drawn from 5V supply is only 0.1 A. 

it had to be 0.4A.

we also connected the TSW1400 board to ADS5294 we are getting TIMED_OUT_ERROR.

Can anyone kindly find the solution for above problem.

Thanks and Regards

Suraj Gaonkar

  • Make sure USB is connected and otherwise, the device might be in power down mode. 

    did your EVM experience any ESD event?look like the EVM is damaged if you saw current from 0.4A to 0.1A under the same condition.  

    Thanks!