Other Parts Discussed in Thread: ADCPRO
Hi Team,
One of my customer is evaluating device EVM and facing issues during evaluation. Customer is using ADS1278-EVM PDK with MM0 Motherboard, faced some error while installing the software but when reinstalled it was fine. The Power adapter is not working hence the MM0 is powered from +5V through J14. The MM0 alone is taking around 80mA and with ADS1278 its taking around 240mA. The MM0 is connected to PC with Windows XP through ADCPro Software. The Test mode and EVM is loaded and its showing "connected". When the data is acquired its showing "collecting data" but no data is displayed. The screen shot of the same is attached for your reference. Can you please help with your comments to address the same.
Thanks in advance for your help and support.
Regards, Shinu Mathew.