Other Parts Discussed in Thread: ADS52J65
I originally opened a ticket on the support page, but was advised to post the question here. In short, the difficulty we are facing is the following:
We would like to use the ADS52J65EVM evaluation board with the TSW14J56 data acquisition module. We have installed the required software packages, but the ADS52J65_EVM_v1.0.0 appears to function only with elevated access rights. I am not talking about the setup/installation file, because it would be OK, if one needed administrator rights for that. However, once the software is installed, it still requires administrator access. Since this is not a viable option for us, I was wondering, whether we could work around the problem.
1. Is there is a version of ADS52J65_EVM that does not require elevated rights? If so, where would one find the download link?
2. If such a version doesn't exist, is it known, what the software has to access with elevated rights? We could then set the registry appropriately.
Thanks,
Zoltán