Hi,
I am facing some confusion while going through the specification of TI ADC (MPN ADS8678).
1. There are 8 ADC channel ( with Associated PGA), what is the AUX_IN terminal in the IC. Is it the ADC without PGA?
2. For each Analog input we can select the input range. What is the PGA gain for each input range selected.
3. Can we change the PGA gain for the input range selected?
Please provide clarification on the raised query?
Regards
Manish