This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC7571: Some quesitons

Part Number: DAC7571

Hi Sirs,

Sorry to bother you.

1. VDD is 5V_STBY, and I2C signal pull up to 3V3 Run, as shown in the figure, please help to confirm whether this behavior is correct? Or I2C also pull up to 3V3_STBY is more suitable?

 

2. As shown schematics, for example U7, we get DAC address as 0x98, but when the power is turned on, but it detects three addresses as 0x3E/0x6C/0x6E. By the way, we use 100KHz standard I2C, please help to confirm.

 

3. Above three addresses 0x3E/0x6C/0x6E, when we command these three addresses, only 0x6C is successfully written, but DAC output has not response.