This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC7528: 4-quadrant operation

Part Number: TLC7528


Hi team,

Customers want to use TLC7528 chip to generate modulation wave: the reference voltage is ±2V, duty cycle 50% square wave, square wave frequency is a fixed frequency between 2-12KHZ; the output is bipolar wave with variable peak value.

Questions:

Can TLC7528's 4-quadrant operation be powered by a single power supply?

Does TI have a 4-quadrant operation ADC chip that can be powered by a single power supply?

The output waveform is similar to the following waveform:

Best Regards,
Amy