Other Parts Discussed in Thread: THS3215, THS3491, THS3217, THS3091, TIDA-00684
We are in the designing phase of a zero-IF based transmitter using DAC5681 with THS3215.
Our required output frequency range is from 1MHz to 50 MHz.
The DAC samples are at 122.88 MSPS with modulated signal with information bandwidth occupying 48 KHz.
We want to generate transmit signal with the combination of DAC5681 and THS3215. We want an output level of 30 dBm from this circuit to drive next Power amplifier stage, which has 50 Ohm input impedance.
Please suggest, whether we can go ahead with this design or any other recommendations..
Please suggest if any documents like schematics and HDL driver available for this application..