I'm not sure how to interface LVDS to SYNC and SYSREF, the datasheet only gives specifications as below:
I have two questions:
- Are these pins internally biased to 0.9V?
- Are they compatible with LVDS?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm not sure how to interface LVDS to SYNC and SYSREF, the datasheet only gives specifications as below:
I have two questions:
Hi Diverger,
Yes, these signals are internally biased to 0.9V.
Yes, you can drive with LVDS.
Best Regards,
Dan
Hi Diverger,
Yes, they are differential inputs. Vih and Vil are the differential swing thresholds ((+) - (-)).
1.3V (Vih) to 0.5 (Vil) represents a max differential swing of 800 mV. This is enough range to support common interfaces like LVDS and LVPECL.
Best Regards,
Dan
Hi Diverger,
The Common Mode Voltage is internally biased to 0.9VDC. The differential swing around the common mode voltage is 1.3V (Max Vih)to 0.5V (Min Vil).
The EVM sets the common mode to 0.95V which is actually higher than the data sheet states, so I would actually just stay with 0.9VDC common mode voltage as the data sheet states.
Best Regards,
Dan
Hi Diverger,
The datasheet doesn't account for a minimum voltage swing for the SYNC. What FPGA will you be using?
Best Regards,
Dan
Hi Diverger,
I believe both 2.5 and 1.8V based LVDS still have the same common mode (1.25V) and differential swing (350 mV), so use which ever one is more convenient for your FPGA. On the ADC34J43EVM, I am able to establish the JESD link without the level shifting resistors, but would still suggest using them for long term use.
Best Regards,
Dan