This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC60004: SLAA869 - adding capcitor to Vref

Part Number: DAC60004

Dear Team

I'm following the design SLAA869 using DAC60004. I have a total of 4 Op Amps to create a uni-polar to bi-polar pulse.

As you see the schematic, initially, I have installed a 180nF capacitor connected to the REF pin for each of the output buffer circuits.

However, previously, I was noticed as;

"It is not necessary to include this capacitor for each circuit. A single 180nF capacitor for the REF pin is sufficient. In fact, there could be some stability risks associated with using 4x."

May I ask why extra capacitors cause stability risks, meaning the stability for the Op Amp?

Since I need to add extra Op Amps with a different DAC IC, I wish to know about this.