This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC5672A: output can't update?

Part Number: DAC5672A
Other Parts Discussed in Thread: DAC5672

The DAC5672 operates in Single-Bus Interleaved mode.
Mode = 0, sleep = 0.

RESETIQ=0,SELECTIQ = 1,


Clkiq and wrtiq are the same 50Mhz continuous clock. DA is a 10Mhz period change data (continuous addition, then loop),changed when Clkiq and wrtiq Negative edge。 However, the output does not change, it output 400mv and 600mv for the A channel, and 900mv and 100mv for the B channel. There is no change after the fpga program is programed. Should it be a 10Mhz cycle change output? What can cause this problem. Thanks