Other Parts Discussed in Thread: ADS1015
I am using TLA2024 to measure differential voltage between AIN2 and AIN3 with following parameters:
ADDR - > GND - Slave address(48h)
VDD - 5V
I2C bus pull up resistor - 10k Ohm
I2C bus clock frequency - 100kHz
9th clock is too slow. Also, TLA2024 doesn't acknowledge, we get NACK on the 9th clock.
There's no response from the TLA2024 when I tried reading the config register.
Also, I can't write to the TLA2024's config register.
Please help me out.
Regards,
Nishil Bhavsar