This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8638: AC voltage measurement on ADS8638

Part Number: ADS8638

Hi,

I am using ADS8638 for the DC Voltage Measurement. Can I use the same to measure AC Voltage Measurement?

Max AC Voltage Range: -4V to 4V

Please do suggest me a DC and AC Voltage supported ADC, if not applicable with ADS8638.

Thanks in Advance

Regards,

Lithesh

  • Hi Lithesh,

    The ADC does not distinguish DC or AC input signal, we have many ADCs which can support bipolar input directly. Before recommending a suitable device to you, what's your AC signal? frequency, type (sinewave, step or others), channels, sampling rate required etc.?

    Thanks&regards,

    Dale